Part Number: PROCESSOR-SDK-J784S4
Tool/software:
Hello Guys,
I plan to boot up EVM using the following sequence:
MCU_ROM -> R5F SBL -> MCU R5F AutosarClassicAppImg -> ATF -> A72 SPL -> A72 UBOOT -> LinuxKernel A72
|
----> MAIN R5F and C7x cores
But i have a couple of questions:
1-During the generation of the SBL image (using SDK-RTOS) i can choose among GP/HS/HLOS, my question is, should i use the HLOS option (or GP/HS are also acceptable?) in this case since i pretend to use SDK-LINUX for A72?
2-Same question but regarding "non_combined" vs "_combined" image type using SDK-RTOS, which should i use (or both are acceptable?) in this case since i pretend to use SDK-LINUX for A72?
Thanks!