This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Getting error while adding apache2 service in my recipe.

Part Number: AM625

Tool/software:

Hi TI team,

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1357371/am625-required-meta-webserver-layer
I followed these link but I am still getting error.

I follows below steps,

1) I disable the CONFIG_HTTPD flag.

-> #CONFIG_HTTPD=y

2) Hit the bitbake command for build.

-> bitbake -c clean acmh-image && bitbake acmh-image

3) Error.

ERROR: acmh-image-1.0-r0 do_rootfs: Postinstall scriptlets of ['busybox'] have failed. If the intention is to defer them to first boot,
then please place them into pkg_postinst_ontarget:${PN} ().
Deferring to first boot via 'exit 1' is no longer supported.
Details of the failure are in /home/alakhara/tisdk/build/arago-tmp-default-glibc/work/am62xx_evm-oe-linux/acmh-image/1.0-r0/temp/log.do_rootfs.
ERROR: Logfile of failure stored in: /home/alakhara/tisdk/build/arago-tmp-default-glibc/work/am62xx_evm-oe-linux/acmh-image/1.0-r0/temp/log.do_rootfs.2055142
ERROR: Task (/home/alakhara/tisdk/sources/meta-custom-acmh/recipes-example/images/acmh-image.bb:do_rootfs) failed with exit code '1'


Please help me out.

  • Hi,

    I just tried the steps to add the 'apache2' webserver package as outlined on the E2E thread you referenced in the context of AM62 SDK v10.0 by extending the IMAGE_INSTALL variable and adding the extra meta-webserver layer and had no issues building images. The only difference I encountered was that the location of the BusyBox config file has changed, so I modified it in the place below:

    $ git -C ../sources/meta-arago/ diff
    diff --git a/meta-arago-distro/recipes-core/busybox/busybox/network.cfg b/meta-arago-distro/recipes-core/busybox/busybox/network.cfg
    index 57499a77..01def934 100644
    --- a/meta-arago-distro/recipes-core/busybox/busybox/network.cfg
    +++ b/meta-arago-distro/recipes-core/busybox/busybox/network.cfg
    @@ -13,7 +13,7 @@ CONFIG_ARPING=y
     CONFIG_BRCTL=y
     CONFIG_FEATURE_BRCTL_FANCY=y
     CONFIG_FEATURE_BRCTL_SHOW=y
    -CONFIG_HTTPD=y
    +#CONFIG_HTTPD=y
     CONFIG_TELNETD=y
     CONFIG_FEATURE_TELNETD_STANDALONE=y
     CONFIG_FEATURE_TFTP_BLOCKSIZE=y

    You should be able to re-create this by setting up your build environment from scratch based on AM62 SDK v10.0 sources and updating the config as above.

    Regards, Andreas