Tool/software:
Dear Sitara HW champs,
In the Table “6-19. MCU_OSC0 Crystal Circuit Requirements” in the AM64x datasheet, it is specified the following :
. When not using the RGMII and/or RMII interfaces, then +/-100 ppm Xtal could be used
. When deriving the AM64x clock out to supply the ETH PHY, then +/-50 ppm Xtal should be used
However, When using an external clock not derived from the AM64x clock for the ETH PHY (RGMII/RMII I/F), could the +/-100 ppm Xtal be used?
Thank you!
Best regards,
Guillaume