This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM620-Q1: Issue with Loading tispl.bin on AM62x SK Board Using SDK 8.06

Part Number: AM620-Q1

Tool/software:

Hi Team,

I am currently using the AM62x SK board with SDK 8.06, following the default configuration without any modifications. During the image loading process, I am encountering an issue where the loading process stops or hangs while attempting to load tispl.bin.

Details:

SDK Version: 8.06

Hardware: AM62x SK Board

Configuration: am62x_evm_r5_defconfig am62x_evm_a53_defconfig

Issue:

tiboot3.bin loads successfully.

When attempting to load tispl.bin, the process hangs, and I am unable to proceed with further image loading or booting.

I have attached the logs & please help us to resolve our issue.

Thanks & Regards,

Yashavantha Gowda

01000000011a0000616d36327800000000000000475020200100010001000100CCCC
U-Boot SPL 2021.01 (Oct 30 2024 - 08:40:34 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from UART
CCxyzModem - CRC mode, 2(SOH)/330(STX)/0(CAN) packets, 4 retries
Loaded 337092 bytes
Loading Environment from MMC... *** Warning - No MMC card found, using default environment

init_env from device 7 not supported!
Starting ATF on ARM64 core...