Other Parts Discussed in Thread: OMAPL138
Hey gang:
I am totaly new to this and don't even know if I am posting this in the right spot, but from reading the forums, I suspect I will find out soon enough.
I have an OMAPL138 EVM board and I just setup my laptop with VirtualBox and installed the host OS and have everything configured to the point I am trying to create an SD card...
I flashed the UBL bootloader
Plugged in the sd card
Ran dmesg and confirmed the sd card being there.
but when I try and use the mksdboot.sh script it fails because it doesn't find the rootfs
dvsdk-da850-omapl138-evm-rootfs.tar.gz
when i look in the script I see where it looks for that file, but I do not see that file in the directory. It does have: arago-base-tisdk-image-da850-omapl138-evm.tar.gz
Do I just change the script to use this???
Help... I have no idea what I am doing with this embedded stuff.
Thanks
Derek