This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: GPIO_0 module reserved GPIOs

Part Number: AM62A7

Tool/software:

In the AM62ax reference manual, it says the following:

"Since MCU_GPIO0_[23:143], GPIO0_[87:143], and GPIO1_[88:143] are reserved in this device, general purpose interface supports up to 198 pins"

What are these pins reserved for? What are the implications of changing the 'ti,ngpio' Device Tree property for the module's node and using these pins. I see no other references to the reservation of these GPIOs and the purpose for doing so in the manual.

Thank you!