This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM DM6446 - u-boot parameters - video bootargs

I having problems with the video bootargs  in U-boot.  One set of parameters will work with some demos/workshop_examples, but not all of them.
I havent found any good documentation on which parameters to use or why.
The closest resource I've found is the link below.  I'm using a Davinci  EVM DM6446,  with the latest kernal and packages for DVSDK_2_0_0_22.
I've re-built most packages.  The u-boot params are set for  TFTP kernal, NFS filesys

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/p/6196/23269.aspx#23269


;JH - this, puts up a green haze and doesn't work with EVM demos
;   this will work with the workshop example  lab07_osd_setup
; sendln 'setenv videocfg video=davincifb:osd0=720x480x16,1350K:osd1=720x480,1350K:vid0=720x480,2025K:vid1=720x480,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

;JH - this works for SWANN monitor - evm demos
; sendln 'setenv videocfg video=davincifb:vid0=0,2500K:vid1=0,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=ntsc'

;JH - this causes demos to not function correctly
; sendln 'setenv videocfg video=davincifb:vid0=720x576x16,2500K:vid1=720x576x16,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

;JH - not working for video_record workshop 
;sendln 'setenv videocfg video=davincifb:osd0=720x480x16,1350K:osd1=720x480x16,1350K:vid0=720x480x16,2025K:vid1=720x480x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

;JH - this did not work either
;sendln 'setenv videocfg video=davincifb:osd0=720x480x16,2025K:osd1=720x480,2025K:vid0=0,2500K:vid1=0,2500K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

;JH - not working with workshop video record example, works with  evm demos
sendln 'setenv videocfg video=davincifb:osd0=720x576x16,2025K:vid0=0,2500K:vid1=0,2500K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'