This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DaVinci EVM DM6446 - worhshop lab7b - video record problem, .

I’m having problems getting the workshop  apps  to run.   I’m stuck on Lab07b_video_record.    I can run the EVM demos successfully, but I have to change the video bootargs to get them to work.

I can get lab07a_osd_setup    to run, but this requires a different  video bootarg  setting.  Below are some video bootargs  that I’ve tired and the output from the

Lab7b  workshop.

 

 

;JH - this, puts up a green haze and doesn't work with EVM demos

;   this will work with the workshop example  lab07_osd_setup, does NOT work

;               sendln 'setenv videocfg video=davincifb:osd0=720x480x16,1350K:osd1=720x480,1350K:vid0=720x480,2025K:vid1=720x480,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

 

;JH - this works for SWANN monitor - evm demos

;               sendln 'setenv videocfg video=davincifb:vid0=0,2500K:vid1=0,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=ntsc'

 

;JH - this causes demos to not function correctly

;               sendln 'setenv videocfg video=davincifb:vid0=720x576x16,2500K:vid1=720x576x16,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

 

;JH - not working for video_record workshop    

;sendln 'setenv videocfg video=davincifb:osd0=720x480x16,1350K:osd1=720x480x16,1350K:vid0=720x480x16,2025K:vid1=720x480x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

 

;JH - this did not work either

;sendln 'setenv videocfg video=davincifb:osd0=720x480x16,2025K:osd1=720x480,2025K:vid0=0,2500K:vid1=0,2500K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

 

;JH - not working with workshop video record example, works with  evm demos

sendln 'setenv videocfg video=davincifb:osd0=720x576x16,2025K:vid0=0,2500K:vid1=0,2500K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC'

 

 

root@192:/opt/workshop# ./app_DEBUG.x470MV

Debug: Initializing video capture device: /dev/video0

Debug:                 Video capture device opened with file descriptor: 4

Debug:                 Capturing 720x480 video

Debug: 3 capture buffers were successfully allocated.

Debug:                 Capture buffer 0, size 884736 mapped to address 0x4016a000

Debug:                 Capture buffer 1, size 884736 mapped to address 0x40242000

Debug:                 Capture buffer 2, size 884736 mapped to address 0x4031a000

Debug: Entering video_thread_fxn processing loop.

Error: fwrite failed to FILE ptr 0x13008

Debug: Exited video_thread_fxn processing loop

Debug: Starting video thread cleanup to return resources to system

Debug: Halted video capture stream on file descriptor 4

Debug:                 unmapped video capture frame, size 884736 located at 0x4016a000

Debug:                 unmapped video capture frame, size 884736 located at 0x40242000

Debug:                 unmapped video capture frame, size 884736 located at 0x4031a000

Debug:                 Closed video capture device (file descriptor 4)

Debug: Closing output file at FILE * 0x13008

Debug: Video thread cleanup complete. Exiting video_thread_fxn

Debug: Video thread exited with FAILURE status

root@192:/opt/workshop#