This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: use SDK10 startup error

Part Number: AM625


Tool/software:

Hello engineer!

Could you please help me check the following startup errors? Where do I need to modify them?

The SDK10 we use has not been modified, and the schematic is also very similar to EVB.

U-Boot SPL 2024.04 (Nov 05 2024 - 15:33:57 +0800)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
SPL initial stack usage: 13392 bytes
Trying to boot from MMC2
Starting ATF on ARM64 core...

NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
NOTICE: BL31: Built : 16:09:05, Feb 9 2024

U-Boot SPL 2024.04 (Nov 05 2024 - 15:35:27 +0800)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
SPL initial stack usage: 1904 bytes
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
Error (-2): cannot determine file size
Trying to boot from MMC2
Error reading cluster
spl_load_image_fat: error reading image u-boot.img, err - -22
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

THX!