Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH
Tool/software:
Hi,
Platform:TDA4VH J784s4-evm(Our company test board cards)
SDK:ti-processor-sdk-linux-adas-j784s4-evm-09_01_00_06
We want to use the USB2.0 functionality of the board. I found that the default USB menuconfig is M, so we added the USB driver.
+CONFIG_USB_CDNS3_SUPPORT=y
+CONFIG_USB_CDNS3=y
cdns3_plat.c reported an error.
[0.6031] xhic-hcd xhci-hcd.0.auto: XHCI Host Controller
[0.6032] xhic-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[18.041] xhic-hcd xhci-hcd.0.auto: can't setup: -110
[18.603] xhic-hcd xhci-hcd.0.auto: USB bus 1 deregistered
[18.043] xhic-hcd: probe of xhci-hcd.0.auto failed with error -110
The DTS:
&usbss0 {
status = "okay";
pinctrl-0 = <&main_usbss0_pins_default>;
pinctrl-names = "default";
ti,vbus-divider;
};
&usb0 {
dr_mode = "otg";
};
USB0_VBUS already has 5v output and is connected to VCC .
USB0_ID is connected to GND.
USB0_DP is connected to D+.
USB0_DM is connected to D-.
Please check my dts configuration.
Thanks