Other Parts Discussed in Thread: CCSTUDIO
Tool/software:
Hi,
The PMIC has been designed with reference to the following link. In the Linux system, command settings can be made to enter Partial I/O mode, and the PMIC GPIO can be triggered to wake up using hardware.
1. The CANUART wake-up part has not been successful. The MCU SDK version is mcu_plus_sdk_am62ax_09_02_00_38. How can I configure the pinmux in CCStudio to allow the MCU CAN or MCU UART to wake up?Is it possible not to set the MCU GPIO status in Linux?
2. Do you have any hardware suggestions? Where should PMIC_LPM_EN0 be connected?
3. The attached configuration is for the wakeup system; is the wake-up setting done here?
Thank you.