This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B-P1: AM6254ATCGHAALW

Part Number: SK-AM62B-P1

Tool/software:

I am currently using AM6254ATCGHAALW, I am able to boot from an micro SD Card, but not booting from FLASH after the SD Card boot configuring the FLASH; the FLASH using is MTFC32GAZAQHD-AAT (NAND Memory) from Micron. it is configured exactly as the EVAL Board and schematic PROC114E3. Is there a bare metal code to use and see if the FLASH is working?

Thank you, Hernando

  • Hi Hernando,

    Can you let us know what Software version are you using to test with?

    Also can you share the output of the below two commands after stopping at u-boot 

    sf probe

    mtd list

    This will help route your query to the right expert.

    Best Regards,

    Suren