Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH
Tool/software:
Dear expert:
My configuration is:
- Serdes0 lane0 & lane 1 : PCIe 1 x2 for EP Xilinx FPGA, 8GT/s
- Serdes0 lane2 & lane 3 : PCIe 3 x1: connects to Intel i226 which is fixed mounted on my TDA4VH board., 5GT/s
Problem:
- Boot up with i226 only, then hot plug in FPGA board, system crash most time, some times not crash, but can't detect FPGA EP, only i226 detected. Observed register value varies when not crash
- Keep FPGA connected: Register 0x02937014 is 0x0200 0009 Register 0x02917014 is 0x1000 0127
- Remove FPGA:: Register 0x02937014 is 0x1000 0113 Register 0x02917014 is 0x0000 0024
- Insert FPGA in advance with I226 together, can boot up successfully, but can only detect FPGA 8GT/s.
its wired, can you help me find what's the problem?
2024-11-06
We made some progress that seems PCIE1 & PCIE 3 have to work as the same speed . when set FPGA FP to 5GT/s(origin : 8GT/s ) TDA4VH can find two device. my case is 5GT/s
Can you help me with this?