This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The set of dm6467T clockrate

Hi

       The dm6467T dataseet says its clockrate is 1G HZ .But  in codec_engine_2_25_05_16/// all_evmDM6467T.tci the clockrate is set as below:

var params = {
    clockRate: 594,
    catalogName: "ti.catalog.c6000",
    deviceName: "DM6467",
    regs: device_regs,
    mem: mem_ext
};

It is the same as the old  dm6467 platform,if i want to improve the performance of dm6467T ,do I need to change the clockrate from 594 to 1000.

If I change to 1000 what other changes do I need to made,thanks.

Regards,

-David