Part Number: TDA4VL-Q1
Other Parts Discussed in Thread: SYSCONFIG, TDA4VM, TDA4VL, TDA4VH
Tool/software:
I am attempting to update the firewall configuration on the eval kit: J721S2XSOMG01EVM. I am using SysConfig (v1.21.2+3837) and the k3-repart-tool included in the SDK: ti-processor-sdk-linux-edgeai-j721s2-evm-10_00_00_08. I copied in the .metadata and data directories from k3-repart-tool in ti-processor-sdk-linux-edgeai-j721s2-evm-09_02_00_05, since they seem to be omitted from 10.0.0.8.
Is there documentation on this tool? For instance:

Also, the TRM indicates the Priv-IDs and Route IDs are defined in the "Appendix Spreadsheet." Is this the spreadsheet that also contains the register definitions? I do not see it there and I don't know what else the "Appendix Spreadsheet" could be a reference to. Please provide a direct link to avoid confusion.
I am also not entirely clear on how the generated file integrates into the bootloader. It's possible that I'm just not seeing the right section in the documentation, so if so, could you please point to it?