This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: tensor maps patch Error

Part Number: TDA4VM


Tool/software:

Hi:

The following error occurred after running 1300 frames of model inference.

Success to open file /opt/vision_apps/invo_alg_model_test/pengzhao/mos/output//1623750065722531.bin for writing!
16228 275.324786 s: VX_ZONE_ERROR:[tivxMapTensorPatch:687] No available tensor maps
275.324790 s: VX_ZONE_ERROR:[tivxMapTensorPatch:688] May need to increase the value of TIVX_TENSOR_MAX_MAPS in tiovx/include/TI/tivx_config.h
tidlObj->num_output_tensors = 1
275.324845 s: VX_ZONE_ERROR:[tivxMapTensorPatch:687] No available tensor maps
275.324848 s: VX_ZONE_ERROR:[tivxMapTensorPatch:688] May need to increase the value of TIVX_TENSOR_MAX_MAPS in tiovx/include/TI/tivx_config.h
file_header 1234 1112 448 448 1 5 2000 220 0 16228
process pic file = /opt/vision_apps/invo_alg_model_test/pengzhao/mos/input/1623750080069088.yuv