Dear all,
Can dm368 do 4CH-D1@30fps MJPEG decode and 4CH-D1@30fps H264 encode simultaneously ? If it is not, the 4CH-D1@20fps H264 encode is the limit, right? Or the former need to reduce the stream frame rate to reach this condition.
The data flow is 4CH-D1@30fps MJPEG decode from ethernet and do the 4CH-D1@30fps H264 encode(transcode) at the same time, then write the file to SD card.
Please help me to confirm this probability. Thanks in advance.
B.R.
Omin