Other Parts Discussed in Thread: AM3715
Hello,
I'm trying to get WEC7 (WinCE7) working on my board.Custom board based on EVM reference board (AM3715 CPU), with 512MB instead of 256mb
I try to boot from SD (and ignore NAND for now as it is 8bit instead of 16bit as on the reference board).SD card contains MLO, EBOOTSD.nb0 and NK.bin
After boot I get the following over uart:
Texas Instruments Windows CE SD X-Loader for EVM 3730
Built Aug 4 2011 at 12:28:13
Version BSP_WINCE_ARM_A8 2.00.00.02
open ebootsd.nb0 file
Init HW: controller RST
SDCardInit: No media found!
BLSDCardDownload: fileio init failed
SD boot failed to open file
HALT
Any help will be greatly appreciated.
regards,
Arthur