This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: About PMIC TPS6521902 and μSD connection for AM6232ASGGHAALW at extended IO port.

Part Number: AM623
Other Parts Discussed in Thread: TCA9555

Tool/software:

Hi team

I want to use extended IO port (TCA9555) with I2C at input of the VSEL_SD and MODE/STBY(configured as STBY) pins for TPS6521902 and μSD reset input.

Are there any limitations to the above use cases?

For example, it is not supported in SDK 8.6, the controls can't keep up, and so on.

CPU is AM6232ASGGHAALW.

Best regards.