This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Baud Rate Adjustment/modification for MCSPI Transaction without Reinitializing

Part Number: TDA4VM

Tool/software:

Hi team,

I am currently working on MCSPI peripheral in TDA4 board. Is there an alternative method to set the baud rate for MCSPI on the TDA4? I’m aware that it can be configured by updating MCSPI_Params.bitrate, but I’m curious if there are other options available.

I would like to update the baud rate for every transaction without reinitializing the MCSPI Instance.

For example, once the MCSPI initialization is completed, I’d like to send data at XYZ Hz, and after that transaction is complete, send another data at ABC Hz— all without deinitializing anything.

How can this be achieved? 

Thanks in advance.