Tool/software:
HI。TEAMS
If the synchronization mode of AM4372 selects 16 bits for data, does it take 16 clock cycles to read 16 bits? Is AM4372 16 bit parallel port parallel to serial?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
HI。TEAMS
If the synchronization mode of AM4372 selects 16 bits for data, does it take 16 clock cycles to read 16 bits? Is AM4372 16 bit parallel port parallel to serial?
Hello SHENG YANG
Thank you for the query.
GPMC is a parallel bus. I would expect the 16 bit data to be read for every clock.
Is AM4372 16 bit parallel port parallel to serial?
Please eloborate.
Regards,
Sreenivasa
HI。Kallikuppa Sreenivasa
Are D0, D1, D2, and D3 in the above diagram 1-bit or 16-bit?
Can the GPMC interface support DMA transfers for 8 channels?
EDMA has a total of 64 channels. When GPMC is reading data, can the data be allocated to 8 of these channels?
Now it is necessary to read data from the FPGA through the GPMC interface. There are 8 packets of data, each packet containing 4 bytes. After GPMC receives the 8 packets of data, can 8 channels of DMA be configured to transfer the data?
Hi,
Closing the thread, as there is no response for long. Feel free to ping back, if you want to continue discussion.
Regards
Ashwani