Hi!
Do you have any plans for SATA support in StarterWare framework?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
Do you have any plans for SATA support in StarterWare framework?
Thanks!
Hi,
There are no plans to support SATA in StarterWare in the near future.
Regards
Baskaran
that is very strange move - to add support for features that could be easyly implemented, and skip support for complex and hard to implement features.
Hi Sergey,
The peripherals to be supported are finalised based on the requirement from the field. We do provide support for complex peripherals like USB, ethernet. If there is a significant requiremetnt for adding SATA support in StarterWare we can consider that.
Regards
Baskaran