This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupt problem in a DM368



Guys,

 

I have setup an interrupt that would fire every 20ms, but is acting very random, below is my code:

I call interruptInit() from Main to run it, and is just acting very random.

 

/********************************************************/
/* Function: interruptInit(void)                        */
/* Interrupt 20ms. INTERVAL_TIME_RESOLUTION sets the    */
/* time. The variable comes from rs485.c                */
/********************************************************/
void interruptInit(void) {

    struct sigaction sa;
    struct itimerval timer;
   
    timerStatus = TRUE;
    memset (&sa, 0, sizeof (sa));
    sa.sa_handler = &timer_handler;
    //sigaction (SIGALRM, &sa, NULL);
    sigaction (SIGPROF, &sa, NULL);

    //Mutiply by 1,000 to make it 20ms
    timer.it_value.tv_sec = 0;
    timer.it_value.tv_usec = INTERVAL_TIME_RESOLUTION * 1000;

    timer.it_interval.tv_sec = 0;
    timer.it_interval.tv_usec = INTERVAL_TIME_RESOLUTION * 1000;

    //setitimer (ITIMER_REAL, &timer, NULL);
    setitimer (ITIMER_PROF, &timer, NULL);

}




/********************************************************/
/* Function: timer_handler (int sinum)                  */
/* Handles the interrupt                                */
/*                                                      */
/********************************************************/
void timer_handler (int sinum) {
    if (timerStatus == TRUE) {
        onInterval();
    }


}