This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: The file system is damaged due to high and low temperature pressure measurement

Part Number: TDA4VM
Other Parts Discussed in Thread: CSD

Tool/software:

1、We took a high and low temperature pressure test for 16 hours and found that our sleep file was damaged after the pressure test

root@j721e-evm:~# ls -l /bin/
[ 7052.671361] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm ls: iget: bad extended attribute block 141733921779
ls: cannot access '/bin/sleep': Structure needs cleaning
lrwxrwxrwx 1 1083 1083     14 Mar 9 2018 sh -> /bin/bash.bash
l????????? ? ?   ?         ?           ? sleep
-rwxr-xr-x 1 1083 1083   39496 Mar 9 2018 sleep.coreutils

2、Compared with the normal sleep file md5, changes were found

root@j721e-evm:~# md5sum /bin/sleep
[ 7183.920146] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm md5sum: iget: bad extended attribute block 141733921779
md5sum: /bin/sleep: Structure needs cleaning
root@j721e-evm:~# md5sum /bin/sleep.coreutils
1cf18ac911052676f370fdcd9ecb71f7 /bin/sleep.coreutils
root@j721e-evm:~# md5sum /run/media/bin/sleep.coreutils  
media/
root@j721e-evm:~# md5sum /run/media/rootfs-mmcblk0p3/bin/sleep.coreutils
1cf18ac911052676f370fdcd9ecb71f7 /run/media/rootfs-mmcblk0p3/bin/sleep.coreutils
root@j721e-evm:~# md5sum /run/media/rootfs-mmcblk0p3/bin/sleep          
1cf18ac911052676f370fdcd9ecb71f7 /run/media/rootfs-mmcblk0p3/bin/sleep
root@j721e-evm:~#

3、log

[  970.942709] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779
[  974.278923] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779
[  974.290866] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779
l[  976.369471] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779
[  976.381406] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779

4、emmc  pressure test after the problem, read and write no abnormal

Start Emmc Test time:56
####################### Thu Apr 28 19:36:29 UTC 2022 ###########################
clock:         200000000 Hz
actual clock:   200000000 Hz
vdd:           7 (1.65 - 1.95 V)
bus mode:       2 (push-pull)
chip select:   0 (don't care)
power mode:     2 (on)
bus width:     3 (8 bits)
timing spec:   9 (mmc HS200)
signal voltage: 1 (1.80 V)
driver type:   0 (driver type B)
Start dd 2048M test.bin
2141192192 bytes (2.1 GB, 2.0 GiB) copied, 54 s, 39.6 MB/s
2048+0 records in
2048+0 records out
2147483648 bytes (2.1 GB, 2.0 GiB) copied, 54.1581 s, 39.7 MB/s
End dd 2048M test.bin
Start rm test.bin
End rm test.bin
eMMC Life Time Estimation A [EXT_CSD_DEVICE_LIFE_TIME_EST_TYP_A]: 0x01
eMMC Life Time Estimation B [EXT_CSD_DEVICE_LIFE_TIME_EST_TYP_B]: 0x01
eMMC Pre EOL information [EXT_CSD_PRE_EOL_INFO]: 0x01
End Emmc Test time:56
######################## Thu Apr 28 19:37:24 UTC 2022 ###########################

5、emmc Model KLM8G1GEUF-B04%