Part Number: SK-AM62
Tool/software:
hi team,
I have successfully written keys to a SK-AM62B development board using (am62x/keys_devel ) default keys and tried with one short certificate , and device changed from HS-FE to HS-SE .
then replaced smpk.pem from am62x/keys_devel with board/ti/keys/custMpk.pem of yocto build ,and rebuild the uboot.
in build folder there are 3 tiboot3 found (gp,hs,hs-fs) i tried with tiboot3-am62x-hs-evm.bin the its getting reset error.
attaching error log below
U-Boot SPL 2023.04-ti-g836606420854 (May 09 2024 - 05:42:45 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.8--v09.02.08 (Kool Koala)')
SPL initial stack usage: 13408 bytes
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
regards,
-RJ