Tool/software:
Dear Sir/Madam,
I use AM3354 in our product to run Linux OS. The board was designed by us with discrete components.
We had run 2 round of prototype build and 30pcs for each round, the boards from both round are runs normally for the Linux OS + application.
Now we are in small batch production phase, however part of them (5 out of 30pcs) have the issue: Bootloader on NOR Flash works well to read the image file from NAND Flash and load to DDR3, the checksum calculation for image file is also pass, however, when jump from boot to Linux, the Linux startup failed. There is no information print out after "jump to Linux". This issue happens occasionally, maybe the Linux startup failed in 3 times out of 10 times power on/off.
Question: Whether you can provide me a checklist for electronic side to investigate this issue, to let me understand which part lead to this issue? What I can do to check or ensure whether this issue is on electronic side?
Thank you.