Part Number: TDA4VEN-Q1
Tool/software:
Hi TI's experts,
HW ENV:TDA4Ven EVM board
SW ENV:SDK10.0
BOOT MODE:SBL BOOT with SD card
After I modify the DDR density from 8g to 4g and using memtester command to test DDR, but the test results were not as expected.
Using the memtester 70M can test successfully.
Using the mentester command exceeds 80M, the console is block and can't exit by using ctrl+c, only by powering off and on can normal operation be restored.

Regards.