Tool/software:
Hi TI's experts,
HW ENV:our own tda4ven board
SW ENV:SDK10.0
BOOT MODE:spl boot with ospi+emmc
Following the OSPI NOR flash steps via 3.1.1.7. OSPI/QSPI — Processor SDK J722S Documentation, I can flash tiboot3.bin, tispl.bin and u-boot.img to ospi nor device and it also boot successfully.
But it seems that the bootmedia can only recognize SD cards and cannot recognize EMMC
How to change bootmedia from sd to emmc when OSPI boot?
Regards.