This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6457 I2C interface Voltage

According to page 87,88,90 in SPRS582B, C6457 I2C interface Voltage should be 1.8V. This means SDA and SCLK should be pulled up to 1.8V with 4.7K resistor. But on page 12 in schematic_C6457evm_r01b4.pdf,  these two pins are pulled up to 3.3V with 4.7K resistor. I'm puzzled by the confliction. Any one has practical experirence with C6457 I2C interface ?

   BR & Thanks

R.J. Lu