Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J722SXH01EVM: [TDA4AEN] Question regarding the use of an HDMI grabber.

Part Number: J722SXH01EVM

Tool/software:

Hello. TI members

I have a question regarding the use of an HDMI grabber.

You can see the grabber information at this LINK.

https://www.avermedia.com/product-detail/GC513

I have two EVM boards with identical OPN and ASSY numbers.

- OPN# : J722SXH01EVM

- ASSY : PROC170E3A(002)

When using the same application and HDMI grabber on both boards, one board displays correctly through the grabber, while the other only shows a "no signal" message.

Upon examining the hardware differences, I discovered that the non-functioning board lacks an HDMI ESD protection device, specifically the chipset located at 'U197' in the schematic.

I got the schematics from this LINK

- https://www.ti.com/lit/zip/sprr495

Additionally, a capacitor at C661, which is associated with the audio codec, is also missing.

Do you think the presence or absence of this chipset could be the root cause of the result I’m facing?

Best regards

Yongsig