This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62P-LP: Microphone connected through 3.5 mm audio jack is treated as audio output.

Part Number: SK-AM62P-LP

Tool/software:

Hi Team,

We are facing another issue while connecting a Sony's microphone (ECM-LV1) through 3.5mm audio jack. It is getting treated as audio output and no audio input is getting captured. And when tried connecting through an audio splitter, then the capture works but audio output does not work most of the time.

Also getting continuous logs of " pcm_open(in) failed:"  and " pcm_open(out) failed:" while trying to capture or play audio.

5355.dmesgLog.txt

Attaching dmesg log as well for reference.

Requesting support to resolve this.

Regards

Biju Menon