This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: AM5728 MCASP internal clock

Part Number: AM5728

Tool/software:

What is the AM5728 MCASP internal clock used for MCASP_TXCLKCHK  (0x4846 40C8) 

 

Transmit clock count value (from previous measurement). The clock
circuit continually counts the number of interface clocks for every 32
transmit high-frequency master clock (AHCLKX) signals, and stores the
count in XCNT until the next measurement is taken

AHCLKX is generated from AUXCLK which I have routed from the output of DPLL_ABE so that works out correctly, but I don't know/can't find the definition of the MCASP interface clock