Part Number: TDA4VH-Q1
Tool/software:
Hello Colleagues,
We were testing our camera pipeline and ISP performance using the IMX390 camera and encountered a greenish tint issue in the image. There are four different images in the shared zip file, representing two different scenes (I can provide more images for further investigation if needed). One pair of images was captured with a camera featuring a built-in ISP, which appears normal (not green). The other pair was captured with a camera without a built-in ISP, where we used the ISP binaries provided in the IMX390 SDK.
In general we have observed that the greenish tint issue occurs on walls, asphalt or grey regions. It is also important to note that it occurs everywhere not just around peripherals or center. Do you have any comments or suggestions on this issue? What could be the root cause of such problem?
Thanks in advance.