Hi ,
We are facing a critical issue which bit rate is oscillating from 600Kbps to 7000Kbps with the same field of view.
Randomly codec algorithm is not working, even though if we create huge motion on the scene, the bit rate is not shoots up and keeps on retaining with 600~1000kbps. After sometime, the same camera bit rate shows an average value of 4500kbps.
Codec lib: 02.00.00.09
Codec algorithm: VBR
initQ = 28;
rcQMax = 35;
rcQMin = 25;
rcQMaxI = 35;
rcQMinI = 25;