Tool/software:
Hi, TI experts,
SDK VERSION:
Linux SDK: 08.04.00.11
RTOS SDK: 08.04.00.06
We produced over 10000, but there were 2 boards that failed to start up.
Board 1:
board1 ddr is init ok, but stuck at copy data to ddr, the probability of startup failure is 100%
We have conducted the following investigation:
1. adjust the cpu voltage from 600mv - 1050mv -- not effect
2. adjust the core voltage from 600mv - 1000mv -- not effect
3. We update below ddr config which is ok at normal board(remove .txt from the file name), but can not help
Copy of SPRACU8B_Jacinto7_DDRSS_RegConfigTool-N50-240429-from TI.xlsb.txt
board2:
board 2 stuck at bl31 init, the probability of startup failure is 100%
we do the voltage adjust as board 1, but can not work.
1. adjust the cpu voltage from 600mv - 1050mv -- not effect
2. adjust the core voltage from 600mv - 1000mv -- not effect
Is there any suggestion to help to location the problem?
Thanks
Ethan