Part Number: AM6422
Tool/software:
Hi,
I'm designing custom board with AM64x.
I may not be able to use UART0 because conflicted the pins with other device that I would like to use.
In this case, UART0 is disabled.
1. Should I enable UART0?
2. If I don't enable UART0, is any limit or problem occurred?
3. Is there other method to get the information that output when UART boot?
4. Are there any other UART ports should not be disabled?
Best Regards,
Koji