Part Number: TDA4VM-Q1
Tool/software:
hello everyone,
when i use sbl to boot by mmcsd in j721e_evm, some errors happened:
1 .compile command: make sbl_mmcsd_img_hlos BOARD=j721e_evm SOC=j721e
2 .then copy *.tiimage to sd card BOOT partition as tiboot3.bin,
3. copy tifs.bin as tifs.bin in BOOT partition.
my uart print :
SBL Revision: 01.00.10.01 (Nov 20 2024 - 13:19:45)
This is SBL , TI SBL Running 1 ...
This is SBL , TI SBL Running 2 ...
TIFS ver: 10.0.8--v10.00.08 (Fiery Fox)
SCISERVER Board Configuration header population... PASSED
Sciclient_setBoardConfigHeader... PASSED
This is SBL , TI SBL Running 3 ...
Efuse xlated: VD 2 to 815 mV (OppVid: 0x3a, Slave:0x48, Res:0x0)
Successfully set voltage to 815 mV for Slave:0x48, Res:0x0
Initlialzing PLLs ...done.
InitlialzingClocks ...done.
Initlialzing DDR ...done.
Initializing SERDES ...done.
Initializing GTC ...
Copying EEPROM content to DDR ...EEPROM Data Copy Done.
This is SBL , TI SBL Running 4 ...
Begin parsing user application
This is SBL ,SBL Running 4-1 ...
Calling Sciclient_procBootRequestProcessor, ProcId 0x20...
Calling Sciclient_procBootRequestProcessor, ProcId 0x21...
Calling Sciclient_procBootRequestProcessor, ProcId 0x1...
Calling Sciclient_procBootRequestProcessor, ProcId 0x2...
Calling Sciclient_procBootRequestProcessor, ProcId 0x6...
Calling Sciclient_procBootRequestProcessor, ProcId 0x7...
Calling Sciclient_procBootRequestProcessor, ProcId 0x8...
Calling Sciclient_procBootRequestProcessor, ProcId 0x9...
Calling Sciclient_procBootRequestProcessor, ProcId 0x3...
Calling Sciclient_procBootRequestProcessor, ProcId 0x4...
Calling Sciclient_procBootRequestProcessor, ProcId 0x30...
SD Boot - File open fails
Sciclient_procBootReleaseProcessor, ProcId 0x20...
Sciclient_procBootReleaseProcessor, ProcId 0x21...
Sciclient_procBootReleaseProcessor, ProcId 0x1...
Sciclient_procBootReleaseProcessor, ProcId 0x2...
Sciclient_procBootReleaseProcessor, ProcId 0x6...
Sciclient_procBootReleaseProcessor, ProcId 0x7...
Sciclient_procBootReleaseProcessor, ProcId 0x8...
Sciclient_procBootReleaseProcessor, ProcId 0x9...
Sciclient_procBootReleaseProcessor, ProcId 0x3...
Sciclient_procBootReleaseProcessor, ProcId 0x4...
Sciclient_procBootReleaseProcessor, ProcId 0x30...
This is SBL ,SBL Running 4-2 ...
as show i set many users uart print:
example: This is SBL ,SBL Running 4-2 .
in source code:

SBL_log(SBL_LOG_MIN, "\n This is SBL ,SBL Running 4-1 ...\n");
SBL_BootImage(&k3xx_evmEntry);
SBL_log(SBL_LOG_MIN, "\nThis is SBL ,SBL Running 4-2 ...\n");
the code enter in SBL_BootImage(&k3xx_evmEntry) , but my print command in this function not work:

also the mcu uart print : SD Boot - File open fail, i set print before this code , but not work,

the sbl was expected print SD Boot - File open fail 1234 but not, somethings error happended,
So why sbl print error, why mmcsd boot not execute code i want , thank you!