This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7-Q1: Se-linux compile issue

Part Number: AM62A7-Q1


Tool/software:

Hi Expert,

customer using below instruction to enable selinux feature:

 SELinux.rst

to enable SELinux permissive and enforcing modes.

 You can use the following to verify if anything seems amiss:

This gist contains the additions to bblayers.conf and local.conf to enable selinux

This patch adds selinux to the builds

This gist adds SELINUX configs to the Linux kernel

This patch adds the SELinux packagegroup to the target I'm building (tisdk-default-image)

but customer encounter some issue when Yocto compile, because of you are using SDK10.0, customer are using SDK9.2, so there is some gap, need you help. could you provide a pre-compiled rootfs? or can you help check the error?

yocto_complile_error.txt

BR,

Biao