This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXEVM8168 HDMI capture

I have a customer evaluating the TMDXEVM8168 board and needs to capture a 1080p30 video stream on an HDMI input port and save it in H264 format. The final goal is to capture 2 streams through 2 HDMI ports.

After testing capture_encode example (supplied with EZSDK) they can capture required video through VIP1_PORTA and VIP2_PORTA (component inputs), but not through HDMI.

According to below post on forum there is no HDMI capturer/receiver with EVM8168 board.

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/139681/503946.aspx#503946

Can anyone confirm if it is possible to capture 1080p30 or 1080p60 video from HDMI ports with EVM8168 ?

If so, is it supported by EZSDK (> 5.02 version)? Is there any source code available?

Thanks in advance.