This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6457(VCP, TCP) simulator in ccs4

Hi,

I want to work on C6457 simulator in ccs4. But the problem is that in CCS4 there is no option in the check list to select this C6457 processor. the closest simulator is for c6455.

Basically i want to work on viterbi coprocessor. i donot have C6457 EVM yet so i need to run stuff on simulator.

so can anyone please tell me that :

1. Is C6457 simulator avaible for CCS4?  If it is then why can i not see it in the list  :-(  and if not then how should i proceed.

2. has anyone run the viterbi coprocessor examples (availible from Texas Instruments ) on CCS4? i checked on CCS3.3 and the example is running but i am not been able to run things on CCS4.

 

Thanks a lot.

Khawar