Part Number: DRA821U-Q1
Tool/software:
Hi,
We encountered an issue during the boot-up process using our own controller: "Unable to handle kernel paging request at virtual address ffff800085ffffff."
Our working environment: 1) SDK version = j7200-evm-10_00_07_03; 2) boot mode = mmcsd, SD is 32G.
Detailed Description of the Issue's Occurrence:
firstly, we build kernel, pdk, and get SBL image, then copy tiboot3.bin, tifs.bin, can_boot_app_mcu_rtos_mcu1_0_release.appimage, tikernelimage_linux.appimage, tidtb_linux.appimage, atf_optee.appimage, lateapp1, lateapp2 to boot patition. and extract tisdk-default-image-j7200-evm.rootfs.tar.xz to the rootfs partition.
After following the first step, the board boots up normally and the UART prints correctly.
However, based on first step, we do another step "make linux_install", An error message appeared on the UART print.
Error information
Finished Reboot and dump vmcore via[ 9.730922] remoteproc remoteproc0: attaching to 41000000.r5f kexec. [ 9.740059] Unable to handle kernel paging request at virtual address ffff800085ffffff [ 9.748301] Mem abort info: [ 9.751254] ESR = 0x0000000096000006 [ 9.760938] EC = 0x25: DABT (current EL), IL = 32 bits [ 9.766532] SET = 0, FnV = 0 [ 9.770025] EA = 0, S1PTW = 0 [ 9.773204] FSC = 0x06: level 2 translation fault [ 9.778409] Data abort info: [ 9.781448] ISV = 0, ISS = 0x00000006, ISS2 = 0x00000000 [ 9.787295] CM = 0, WnR = 0, TnD = 0, TagAccess = 0 [ 9.792528] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0 [ 9.803074] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000081039000 [ 9.820219] [ffff800085ffffff] pgd=10000008fffff003, p4d=10000008fffff003, pud=10000008ffffe003, pmd=0000000000000000 [ 9.838067] Internal error: Oops: 0000000096000006 [#1] PREEMPT SMP [ 9.844343] Modules linked in: phy_can_transceiver ti_k3_r5_remoteproc(+) m_can_platform at24 m_can k3_j72xx_bandgap sa2ul authenc can_dev ti_am335x6 [ 9.864324] CPU: 0 PID: 154 Comm: (udev-worker) Not tainted 6.6.32-g794368ea1434-dirty #5 [ 9.872483] Hardware name: Texas Instruments J7200 EVM (DT) [ 9.878038] pstate: 00000005 (nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 9.884982] pc : rproc_handle_resources.constprop.0+0x64/0x18c [ 9.890814] lr : rproc_boot+0x37c/0x57c [ 9.894646] sp : ffff800081cf36a0 [ 9.897951] x29: ffff800081cf36a0 x28: ffff000805e35280 x27: ffff00080506e880 [2024-11-21 11:19:53 [ 9.905075] x26: ffff00080506e880 x25: 0000000000000001 x24: ffff800085ffffff [ 9.912197] x23: 0000000000000000 x22: ffff000802643838 x21: ffff8000813b4118 [ 9.919320] x20: 0000000000000000 x19: ffff000802643800 x18: 0000000000000000 [ 9.926443] x17: 0000000000000000 x16: 0000000000000000 x15: fbfffffff7ffffff [ 9.933565] x14: fffffbff77ffdfff x13: fbfffffff7ffffff x12: fffffbff77ffdfff [ 9.940687] x11: ffffffffffbfffff x10: ff7fffffffffffff x9 : ffffffffffffffff [ 9.947808] x8 : fffffffdffbfffbf x7 : ffffffffffffffff x6 : fffffffffffeffff [ 9.954929] x5 : ffff000805e9f600 x4 : ffff800086000000 x3 : 00000000000000fd [ 9.962051] x2 : 00000000ffffffff x1 : ffff800086000003 x0 : ffff800086000000 [ 9.969174] Call trace: [ 9.971612] rproc_handle_resources.constprop.0+0x64/0x18c [ 9.977093] rproc_boot+0x37c/0x57c [ 9.977776] m_can_platform 40568000.can: m_can device registered (irq=536, version=32) [ 9.980575] rproc_add+0x184/0x190 [ 9.980582] k3_r5_probe+0x794/0xd3c [ti_k3_r5_remoteproc] [ 9.980598] platform_probe+0x68/0xc4 [ 9.980605] really_probe+0x148/0x2b0 [ 9.980609] __driver_probe_device+0x78/0x12c [ 9.980612] driver_probe_device+0xd8/0x15c [ 9.980615] __driver_attach+0x90/0x19c [ 10.016987] bus_for_each_dev+0x7c/0xdc [ 10.020821] driver_attach+0x24/0x30 [ 10.024390] bus_add_driver+0xe8/0x1f8 [ 10.028134] driver_register+0x5c/0x124 [ 10.031961] __platform_driver_register+0x28/0x34 [ 10.036655] k3_r5_rproc_driver_init+0x20/0x1000 [ti_k3_r5_remoteproc] [ 10.043181] do_one_initcall+0x80/0x1c8 [ 10.047011] do_init_module+0x58/0x1e0 [ 10.050755] load_module+0x1c8c/0x1d18 [ 10.054498] init_module_from_file+0x88/0xcc [ 10.058761] __arm64_sys_finit_module+0x1dc/0x2e4 [ 10.063460] invoke_syscall+0x48/0x114 [ 10.067204] el0_svc_common.constprop.0+0xc0/0xe0 [ 10.071902] do_el0_svc+0x1c/0x28 [ 10.075213] el0_svc+0x2c/0x84 [ 10.078262] el0t_64_sync_handler+0x120/0x12c [ 10.082610] el0t_64_sync+0x190/0x194 [ 10.086272] Code: 6b020063 8b22c098 91001301 540007c4 (b862c880) [ 10.092351] ---[ end trace 0000000000000000 ]--- [ OK ] Reached target Socket Units. [ OK ] Reached target Basic System. [ 10.142552] m_can_platform 2701000.can main_mcan0: renamed from can0 [ OK ] Started Job spooling tools. [ 10.183623] m_can_platform 40528000.can mcu_mcan0: renamed from can1 [ OK ] Started Periodic Command Scheduler. [ 10.216339] m_can_platform 40568000.can mcu_mcan1: renamed from can2
Complete log information:
OTICE: BL31: Built : 16:09:05, Feb 9 2024
I/TC:
I/TC: OP-TEE version: 4.2.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Apr 12 09:51:21 UTC 2024 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot
[2024-11-21 11:19:43
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[2024-11-21 11:19:47
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 6.6.32-g794368ea1434-dirty (igs@igs) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #5 SMP PRE4
[ 0.000000] KASLR disabled due to lack of seed
[ 0.000000] Machine model: Texas Instruments J7200 EVM
[ 0.000000] efi: UEFI not found.
[ 0.000000] [Firmware Bug]: Kernel image misaligned at boot, please fix your bootloader!
[ 0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a0000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a0ffffff (15360 KiB) nomap non-reusable r5f-memory@a0100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a1000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable r5f-memory@a1100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a2000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a2ffffff (15360 KiB) nomap non-reusable r5f-memory@a2100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a3000000..0x00000000a30fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a3000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a3100000..0x00000000a3ffffff (15360 KiB) nomap non-reusable r5f-memory@a3100000
[ 0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a47fffff (8192 KiB) nomap non-reusable ipc-memories@a4000000
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a47fffff]
[ 0.000000] node 0: [mem 0x00000000a4800000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] cma: Reserved 32 MiB at 0x00000000fe000000 on node -1
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.4
[ 0.000000] percpu: Embedded 20 pages/cpu s42920 r8192 d30808 u81920
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Spectre-v3a
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: detected: ARM erratum 1742098
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Kernel command line: console=ttyS2,115200n8 root=/dev/mmcblk1p2 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 2.
[ 0.000000] software IO TLB: mapped [mem 0x00000000fa000000-0x00000000fe000000] (64MB)
[ 0.000000] Memory: 3896276K/4194304K available (11968K kernel code, 1250K rwdata, 4032K rodata, 2432K init, 502K bss, 265260K reserved, 32768K cma-)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000880040000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.000162] Console: colour dummy device 80x25
[ 0.000190] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.000196] pid_max: default: 32768 minimum: 301
[ 0.000238] LSM: initializing lsm=capability,integrity
[ 0.000296] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.000314] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.001193] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.001245] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.001366] rcu: Hierarchical SRCU implementation.
[2024-11-21 11:19:48
[ 0.001368] rcu: Max phase no-delay instances is 1000.
[ 0.001543] Platform MSI: msi-controller@1820000 domain created
[ 0.001658] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.001771] EFI services will not be available.
[ 0.001883] smp: Bringing up secondary CPUs ...
[ 0.010406] Detected PIPT I-cache on CPU1
[ 0.010457] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.010472] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000
[ 0.010504] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.010559] smp: Brought up 1 node, 2 CPUs
[ 0.010563] SMP: Total of 2 processors activated.
[ 0.010566] CPU features: detected: 32-bit EL0 Support
[ 0.010569] CPU features: detected: CRC32 instructions
[ 0.010607] CPU: All CPU(s) started at EL2
[ 0.010608] alternatives: applying system-wide alternatives
[ 0.011433] devtmpfs: initialized
[ 0.016384] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.016398] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.017001] pinctrl core: initialized pinctrl subsystem
[ 0.017249] DMI not present or invalid.
[ 0.017575] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.018207] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.018312] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.018435] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.018469] audit: initializing netlink subsys (disabled)
[ 0.018577] audit: type=2000 audit(0.016:1): state=initialized audit_enabled=0 res=1
[ 0.018774] thermal_sys: Registered thermal governor 'step_wise'
[ 0.018777] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.018797] cpuidle: using governor menu
[ 0.018866] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.018900] ASID allocator initialised with 65536 entries
[ 0.027279] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@100000/pinctrl@a40000/mcu-cpsw-cpts
[ 0.028275] Modules: 27680 pages in range for non-PLT usage
[ 0.028279] Modules: 519200 pages in range for PLT usage
[ 0.028722] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.028726] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.028729] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.028731] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.028734] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.028736] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.028738] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.028740] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.029530] k3-chipinfo 43000014.chipid: Family:J7200 rev:SR2.0 JTAGID[0x1bb6d02f] Detected
[ 0.030413] iommu: Default domain type: Translated
[ 0.030418] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.030554] SCSI subsystem initialized
[ 0.030734] usbcore: registered new interface driver usbfs
[ 0.030745] usbcore: registered new interface driver hub
[ 0.030760] usbcore: registered new device driver usb
[ 0.030978] pps_core: LinuxPPS API ver. 1 registered
[ 0.030981] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.030990] PTP clock support registered
[ 0.031088] EDAC MC: Ver: 3.0.0
[ 0.031339] scmi_core: SCMI protocol bus registered
[ 0.031477] FPGA manager framework
[ 0.031525] Advanced Linux Sound Architecture Driver Initialized.
[ 0.031961] vgaarb: loaded
[ 0.032165] clocksource: Switched to clocksource arch_sys_counter
[ 0.032290] VFS: Disk quotas dquot_6.6.0
[ 0.032305] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.035353] NET: Registered PF_INET protocol family
[ 0.035599] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.037072] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.037103] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.037117] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.037258] TCP bind hash table entries: 32768 (order: 8, 1048576 bytes, linear)
[ 0.038376] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.038524] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.038580] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.038718] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.039041] RPC: Registered named UNIX socket transport module.
[ 0.039047] RPC: Registered udp transport module.
[ 0.039049] RPC: Registered tcp transport module.
[ 0.039050] RPC: Registered tcp-with-tls transport module.
[ 0.039053] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.039058] NET: Registered PF_XDP protocol family
[ 0.039073] PCI: CLS 0 bytes, default 64
[ 0.039769] Initialise system trusted keyrings
[ 0.039893] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[ 0.040059] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.040237] NFS: Registering the id_resolver key type
[ 0.040273] Key type id_resolver registered
[ 0.040275] Key type id_legacy registered
[ 0.040285] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.040288] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.053937] Key type asymmetric registered
[ 0.053941] Asymmetric key parser 'x509' registered
[ 0.053970] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.053974] io scheduler mq-deadline registered
[ 0.053976] io scheduler kyber registered
[ 0.053999] io scheduler bfq registered
[ 0.055738] pinctrl-single 4301c000.pinctrl: 13 pins, size 52
[ 0.055846] pinctrl-single 4301c038.pinctrl: 2 pins, size 8
[ 0.055930] pinctrl-single 4301c068.pinctrl: 59 pins, size 236
[ 0.056206] pinctrl-single 4301c174.pinctrl: 8 pins, size 32
[ 0.056349] pinctrl-single 104200.pinctrl: 20 pins, size 80
[ 0.056419] pinctrl-single 104280.pinctrl: 8 pins, size 32
[ 0.056506] pinctrl-single 11c000.pinctrl: 67 pins, size 268
[ 0.056750] pinctrl-single 11c11c.pinctrl: 3 pins, size 12
[ 0.057144] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[ 0.060498] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[ 0.065515] loop: module loaded
[ 0.066093] megasas: 07.725.01.00-rc1
[ 0.067856] tun: Universal TUN/TAP device driver, 1.6
[ 0.068449] VFIO - User Level meta-driver version: 0.3
[ 0.069057] usbcore: registered new interface driver usb-storage
[ 0.069392] i2c_dev: i2c /dev entries driver
[ 0.070013] sdhci: Secure Digital Host Controller Interface driver
[ 0.070016] sdhci: Copyright(c) Pierre Ossman
[ 0.070131] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.070438] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.070596] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.071000] usbcore: registered new interface driver usbhid
[ 0.071002] usbhid: USB HID core driver
[ 0.071813] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.072073] optee: probing for conduit method.
[ 0.072088] optee: revision 4.2 (12d7c4ee)
[ 0.088544] optee: dynamic shared memory is enabled
[ 0.088979] random: crng init done
[ 0.089034] optee: initialized driver
[ 0.090224] NET: Registered PF_PACKET protocol family
[ 0.090267] Key type dns_resolver registered
[ 0.093825] registered taskstats version 1
[ 0.094022] Loading compiled-in X.509 certificates
[ 0.101188] ti-sci 44083000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[ 0.164942] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.165614] pca953x 1-0021: supply vcc not found, using dummy regulator
[ 0.165676] pca953x 1-0021: using no AI
[ 1.172167] omap_i2c 2000000.i2c: timeout waiting for bus ready
[ 1.172175] pca953x 1-0021: failed writing register
[ 1.172239] pca953x: probe of 1-0021 failed with error -16
[ 1.172392] pca953x 1-0020: supply vcc not found, using dummy regulator
[ 1.172453] pca953x 1-0020: using no AI
[ 2.180167] omap_i2c 2000000.i2c: timeout waiting for bus ready
[ 2.180173] pca953x 1-0020: failed writing register
[ 2.180222] pca953x: probe of 1-0020 failed with error -16
[ 2.180362] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 2.180407] pca953x 1-0022: using AI
[ 3.188167] omap_i2c 2000000.i2c: timeout waiting for bus ready
[ 3.188171] pca953x 1-0022: failed writing register
[ 3.188215] pca953x: probe of 1-0022 failed with error -16
[ 3.188255] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz
[ 3.188852] pca953x 2-0020: supply vcc not found, using dummy regulator
[ 3.188903] pca953x 2-0020: using no AI
[ 4.196175] omap_i2c 2010000.i2c: timeout waiting for bus ready
[ 4.196182] pca953x 2-0020: failed writing register
[ 4.196244] pca953x: probe of 2-0020 failed with error -16
[ 4.196289] omap_i2c 2010000.i2c: bus 2 rev0.12 at 400 kHz
[ 4.196410] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 137 domain created
[ 4.196625] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 131 domain created
[ 4.196712] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 213 domain created
[ 4.196859] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 209 created
[ 4.199653] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,32] sci-dev-id:235
[ 4.199662] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 4.199665] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[ 4.202696] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[120,200] sci-dev-id:211
[ 4.202704] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 4.202707] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[ 4.203401] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 268, base_baud = 6000000) is a 8250
[ 4.204046] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 269, base_baud = 3000000) is a 8250
[ 4.204079] printk: console [ttyS2] enabled
[ 5.840523] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 270, base_baud = 3000000) is a 8250
[ 5.849766] 2830000.serial: ttyS5 at MMIO 0x2830000 (irq = 271, base_baud = 3000000) is a 8250
[ 5.859579] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 5.904169] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[2024-11-21 11:19:49
[ 5.912168] mdio_bus 46000f00.mdio: MDIO device at address 0 is missing.
[ 5.918879] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[ 5.931728] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 5.938937] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 5.945144] pps pps0: new PPS source ptp0
[ 5.949301] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[ 5.959682] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[ 5.968472] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc8900
[ 5.968648] mmc0: CQHCI version 5.10
[ 5.978585] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc8900
[ 6.012217] tps6594 0-0048: error -EREMOTEIO: Failed to set PMIC state
[ 6.016715] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[ 6.018769] tps6594: probe of 0-0048 failed with error -121
[ 6.031918] tps6594 0-004c: error -EREMOTEIO: Failed to set PMIC state
[ 6.038457] tps6594: probe of 0-004c failed with error -121
[ 6.045804] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[ 6.056028] ti-udma 31150000.dma-controller: Channels: 50 (tchan: 25, rchan: 25, gp-rflow: 8)
[ 6.067758] spi-nor spi0.0: unrecognized JEDEC id bytes: 80 00 00 00 00 00
[ 6.075074] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 6.109878] mmc0: Command Queue Engine enabled
[ 6.114334] mmc0: new HS400 MMC card at address 0001
[ 6.119625] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
[ 6.120180] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 6.125060] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB
[ 6.132094] mdio_bus 46000f00.mdio: MDIO device at address 0 is missing.
[ 6.137270] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB
[ 6.143320] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[ 6.148759] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (239:0)
[ 6.161032] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 6.174391] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 6.180596] pps pps0: new PPS source ptp1
[ 6.184748] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[ 6.200743] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 6.211527] debugfs: Directory 'pd:49' with parent 'pm_genpd' already present!
[ 6.211614] mmc1: CQHCI version 5.10
[ 6.220061] debugfs: Directory 'pd:35' with parent 'pm_genpd' already present!
[ 6.229982] clk: Disabling unused clocks
[ 6.245760] ALSA device list:
[ 6.248730] No soundcards found.
[ 6.262779] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[ 6.270372] Waiting for root device /dev/mmcblk1p2...
[ 6.324859] mmc1: new ultra high speed SDR104 SDHC card at address 5048
[ 6.331884] mmcblk1: mmc1:5048 SD32G 29.7 GiB
[ 6.338085] mmcblk1: p1 p2
[ 6.355454] EXT4-fs (mmcblk1p2): mounted filesystem 6bd841d1-9f94-44fa-8a8b-4e60e339874d r/w with ordered data mode. Quota mode: none.
[ 6.367566] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 6.376450] devtmpfs: mounted
[ 6.380917] Freeing unused kernel memory: 2432K
[ 6.385529] Run /sbin/init as init process
[ 6.575336] systemd[1]: System time before build time, advancing clock.
[ 6.617003] NET: Registered PF_INET6 protocol family
[ 6.622539] Segment Routing with IPv6
[ 6.626217] In-situ OAM (IOAM) with IPv6
[ 6.653872] systemd[1]: systemd 255.4^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BL)
[ 6.685672] systemd[1]: Detected architecture arm64.
Welcome to Arago 2023.10!
[ 6.706475] systemd[1]: Hostname set to <j7200-evm>.
[ 6.897725] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Ple.
[2024-11-21 11:19:50
[ 6.959491] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Plea.
[ 7.008020] systemd[1]: Queued start job for default target Graphical Interface.
[ 7.043126] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 7.065452] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 7.089329] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 7.113060] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 7.136412] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 7.160333] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 7.184255] systemd[1]: Expecting device /dev/ttyS2...
Expecting device /dev/ttyS2...
[ 7.200279] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 7.216231] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 7.236220] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 7.252234] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 7.295162] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 7.320332] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 7.345995] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 7.368449] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 7.392829] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 7.416572] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 7.436576] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 7.456616] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 7.484878] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 7.504541] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 7.524520] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 7.568416] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 7.590443] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 7.616550] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 7.632555] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[ 7.648280] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 7.687945] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes 7.697293] systemd[1]: Starting Load Kernel Module configfs...
m...
Starting Load Kernel Module configfs...
[ 7.747827] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 7.773116] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 7.814135] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 7.823408] fuse: init (API version 7.39)
[ 7.832464] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[ 7.866239] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 7.892984] systemd[1]: Starting Load Kernel Modules...
[2024-11-21 11:19:51
Starting Load Kernel Modules...
[ 7.922552] systemd-journald[107]: Collecting audit messages is enabled.
[ 7.932800] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network units from Kernel command line...
[ 7.973495] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 8.001839] systemd[1]: Starting Coldplug All udev Devices...
[ 8.007799] EXT4-fs (mmcblk1p2): re-mounted 6bd841d1-9f94-44fa-8a8b-4e60e339874d r/w. Quota mode: none.
Starting Coldplug All udev Devices...
[ 8.036667] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 8.056643] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Load Kernel Modules.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 8.395014] systemd-journald[107]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev gracefully...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev gracefully.
Starting Create Static Device Nodes in /dev...
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /var/volatile...
[ 8.657684] audit: type=1334 audit(1709054766.080:2): prog-id=6 op=LOAD
[ 8.664720] audit: type=1334 audit(1709054766.088:3): prog-id=7 op=LOAD
Starting Rule-based Manager for Device Events and Files...
[ OK ] Mounted /var/volatile.
Starting Load/Save OS Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Finished Load/Save OS Random Seed.
[2024-11-21 11:19:52
[ OK ] Finished Create Volatile Files and Directories.
[ 8.954585] audit: type=1334 audit(1709054766.376:4): prog-id=8 op=LOAD
[FAILED] Failed to start Network Name Resolution.
See 'systemctl status systemd-resolved.service' for details.
[ OK ] Reached target Host and Network Nam[ 9.001290] audit: type=1334 audit(1709054766.424:5): prog-id=8 op=UNLOAD
e Lookups.
[ 9.025209] audit: type=1334 audit(1709054766.448:6): prog-id=9 op=LOAD
[FAILED] Failed to start Network Time Sync[ 9.036430] audit: type=1334 audit(1709054766.460:7): prog-id=9 op=UNLOAD
hronization.
See 'systemctl status systemd-timesyncd.service' for details.
[ OK ] Reached target System Time Set.
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Found device /dev/ttyS2.
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ 9.226507] audit: type=1334 audit(1709054766.648:8): prog-id=10 op=LOAD
[FAILED] Failed to start Network Name Resolution.
[ 9.248648] audit: type=1334 audit(1709054766.672:9): prog-id=10 op=UNLOAD
See 'systemctl status systemd-resolved.service' for details.
[ 9.275250] audit: type=1334 audit(1709054766.696:10): prog-id=11 op=LOAD
[FAILED] Failed to start Network Time Synchronization.
[ 9.296743] audit: type=1334 audit(1709054766.720:11): prog-id=11 op=UNLOAD
See 'systemctl status systemd-timesyncd.service' for details.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on PC/SC Smart Card Daemon Activation Socket.
Starting Weston socket...
[ 9.509716] CAN device driver interface
[FAILED] Failed to start D-Bus System Message Bus.
See 'systemctl status dbus-broker.service' for details.
[ 9.563951] at24 0-0050: supply vcc not found, using dummy regulator
Starting Reboot and dump vmcore via kexec...
[ 9.648374] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ OK ] Listening on Docker Socket for the [ 9.660453] ti-udma 285c0000.dma-controller: chan1: is running!
API.
[ 9.671664] platform 41000000.r5f: configured R5F for IPC-only mode
[ 9.679284] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[ 9.694017] m_can_platform 2701000.can: m_can device registered (irq=533, version=32)
[ OK ] Listening on Weston socket.
[ 9.702269] remoteproc remoteproc0: 41000000.r5f is available
[ 9.708217] m_can_platform 40528000.can: m_can device registered (irq=534, version=32)
[ OK ] Finished Reboot and dump vmcore via[ 9.730922] remoteproc remoteproc0: attaching to 41000000.r5f
kexec.
[ 9.740059] Unable to handle kernel paging request at virtual address ffff800085ffffff
[ 9.748301] Mem abort info:
[ 9.751254] ESR = 0x0000000096000006
[ 9.760938] EC = 0x25: DABT (current EL), IL = 32 bits
[ 9.766532] SET = 0, FnV = 0
[ 9.770025] EA = 0, S1PTW = 0
[ 9.773204] FSC = 0x06: level 2 translation fault
[ 9.778409] Data abort info:
[ 9.781448] ISV = 0, ISS = 0x00000006, ISS2 = 0x00000000
[ 9.787295] CM = 0, WnR = 0, TnD = 0, TagAccess = 0
[ 9.792528] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[ 9.803074] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000081039000
[ 9.820219] [ffff800085ffffff] pgd=10000008fffff003, p4d=10000008fffff003, pud=10000008ffffe003, pmd=0000000000000000
[ 9.838067] Internal error: Oops: 0000000096000006 [#1] PREEMPT SMP
[ 9.844343] Modules linked in: phy_can_transceiver ti_k3_r5_remoteproc(+) m_can_platform at24 m_can k3_j72xx_bandgap sa2ul authenc can_dev ti_am335x6
[ 9.864324] CPU: 0 PID: 154 Comm: (udev-worker) Not tainted 6.6.32-g794368ea1434-dirty #5
[ 9.872483] Hardware name: Texas Instruments J7200 EVM (DT)
[ 9.878038] pstate: 00000005 (nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 9.884982] pc : rproc_handle_resources.constprop.0+0x64/0x18c
[ 9.890814] lr : rproc_boot+0x37c/0x57c
[ 9.894646] sp : ffff800081cf36a0
[ 9.897951] x29: ffff800081cf36a0 x28: ffff000805e35280 x27: ffff00080506e880
[2024-11-21 11:19:53
[ 9.905075] x26: ffff00080506e880 x25: 0000000000000001 x24: ffff800085ffffff
[ 9.912197] x23: 0000000000000000 x22: ffff000802643838 x21: ffff8000813b4118
[ 9.919320] x20: 0000000000000000 x19: ffff000802643800 x18: 0000000000000000
[ 9.926443] x17: 0000000000000000 x16: 0000000000000000 x15: fbfffffff7ffffff
[ 9.933565] x14: fffffbff77ffdfff x13: fbfffffff7ffffff x12: fffffbff77ffdfff
[ 9.940687] x11: ffffffffffbfffff x10: ff7fffffffffffff x9 : ffffffffffffffff
[ 9.947808] x8 : fffffffdffbfffbf x7 : ffffffffffffffff x6 : fffffffffffeffff
[ 9.954929] x5 : ffff000805e9f600 x4 : ffff800086000000 x3 : 00000000000000fd
[ 9.962051] x2 : 00000000ffffffff x1 : ffff800086000003 x0 : ffff800086000000
[ 9.969174] Call trace:
[ 9.971612] rproc_handle_resources.constprop.0+0x64/0x18c
[ 9.977093] rproc_boot+0x37c/0x57c
[ 9.977776] m_can_platform 40568000.can: m_can device registered (irq=536, version=32)
[ 9.980575] rproc_add+0x184/0x190
[ 9.980582] k3_r5_probe+0x794/0xd3c [ti_k3_r5_remoteproc]
[ 9.980598] platform_probe+0x68/0xc4
[ 9.980605] really_probe+0x148/0x2b0
[ 9.980609] __driver_probe_device+0x78/0x12c
[ 9.980612] driver_probe_device+0xd8/0x15c
[ 9.980615] __driver_attach+0x90/0x19c
[ 10.016987] bus_for_each_dev+0x7c/0xdc
[ 10.020821] driver_attach+0x24/0x30
[ 10.024390] bus_add_driver+0xe8/0x1f8
[ 10.028134] driver_register+0x5c/0x124
[ 10.031961] __platform_driver_register+0x28/0x34
[ 10.036655] k3_r5_rproc_driver_init+0x20/0x1000 [ti_k3_r5_remoteproc]
[ 10.043181] do_one_initcall+0x80/0x1c8
[ 10.047011] do_init_module+0x58/0x1e0
[ 10.050755] load_module+0x1c8c/0x1d18
[ 10.054498] init_module_from_file+0x88/0xcc
[ 10.058761] __arm64_sys_finit_module+0x1dc/0x2e4
[ 10.063460] invoke_syscall+0x48/0x114
[ 10.067204] el0_svc_common.constprop.0+0xc0/0xe0
[ 10.071902] do_el0_svc+0x1c/0x28
[ 10.075213] el0_svc+0x2c/0x84
[ 10.078262] el0t_64_sync_handler+0x120/0x12c
[ 10.082610] el0t_64_sync+0x190/0x194
[ 10.086272] Code: 6b020063 8b22c098 91001301 540007c4 (b862c880)
[ 10.092351] ---[ end trace 0000000000000000 ]---
[ OK ] Reached target Socket Units.
[ OK ] Reached target Basic System.
[ 10.142552] m_can_platform 2701000.can main_mcan0: renamed from can0
[ OK ] Started Job spooling tools.
[ 10.183623] m_can_platform 40528000.can mcu_mcan0: renamed from can1
[ OK ] Started Periodic Command Scheduler.
[ 10.216339] m_can_platform 40568000.can mcu_mcan1: renamed from can2
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting Expand the rootfs partiti…to full size of the boot device....
[ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
[FAILED] Failed to start User Login Management.
See 'systemctl status systemd-logind.service' for details.
[FAILED] Failed to start Network Name Resolution.
See 'systemctl status systemd-resolved.service' for details.
Starting Avahi mDNS/DNS-SD Stack...
[FAILED] Failed to start Network Time Synchronization.
See 'systemctl status systemd-timesyncd.service' for details.
Starting Telnet Server...
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Finished Telnet Server.
[ OK ] Reached target Preparation for Network.
[FAILED] Failed to start D-Bus System Message Bus.
See 'systemctl status dbus-broker.service' for details.
Starting Load Kernel Module drm...
Starting Network Configuration...
[FAILED] Failed to start Network Name Resolution.
See 'systemctl status systemd-resolved.service' for details.
[FAILED] Failed to start Network Time Synchronization.
See 'systemctl status systemd-timesyncd.service' for details.
Starting Virtual Console Setup...
[ OK ] Finished Load Kernel Module drm.
[FAILED] Failed to start D-Bus System Message Bus.
See 'systemctl status dbus-broker.service' for details.
[FAILED] Failed to start User Login Management.
See 'systemctl status systemd-logind.service' for details.
[FAILED] Failed to start Network Name Resolution.
See 'systemctl status systemd-resolved.service' for details.
[FAILED] Failed to start Network Time Synchronization.
See 'systemctl status systemd-timesyncd.service' for details.
[FAILED] Failed to start D-Bus System Message Bus.
See 'systemctl status dbus-broker.service' for details.
Starting Load Kernel Module drm...
[FAILED] Failed to start Network Name Resolution.
See 'systemctl status systemd-resolved.service' for details.
[FAILED] Failed to start Network Time Synchronization.
See 'systemctl status systemd-timesyncd.service' for details.
[FAILED] Failed to start D-Bus System Message Bus.
See 'systemctl status dbus-broker.service' for details.
Starting User Database Manager...
[FAILED] Failed to start D-Bus System Message Bus.
See 'systemctl status dbus-broker.service' for details.
[ OK ] Started Telephony service.
[ OK ] Finished Load Kernel Module drm.
[FAILED] Failed to start User Login Management.
See 'systemctl status systemd-logind.service' for details.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Load Kernel Module drm...
[ OK ] Finished Expand the rootfs partition to full size of the boot device..
[ OK ] Finished Load Kernel Module drm.
[FAILED] Failed to start User Login Management.
See 'systemctl status systemd-logind.service' for details.
Starting Load Kernel Module drm...
[ OK ] Started User Database Manager.
[ OK ] Finished Load Kernel Module drm.
[FAILED] Failed to start User Login Management.
See 'systemctl status systemd-logind.service' for details.
Starting Load Kernel Module drm...
[FAILED] Failed to start D-Bus System Message Bus.
See 'systemctl status dbus-broker.service' for details.
[ OK ] Finished Load Kernel Module drm.
[FAILED] Failed to start Avahi mDNS/DNS-SD Stack.
See 'systemctl status avahi-daemon.service' for details.
[FAILED] Failed to start User Login Management.
See 'systemctl status systemd-logind.service' for details.
[2024-11-21 11:19:54
[ OK ] Finished Virtual Console Setup.
[ 11.004470] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ 11.025732] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 11.033511] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ OK ] Created slice Slice /system/systemd-fsck.
Expecting device /dev/mmcblk1p1...
[ OK ] Started Network Configuration.
[ OK ] Reached target Network.
Starting Enable and configure wl18xx bluetooth stack...
Starting containerd container runtime...
[ OK ] Started Netperf Benchmark Server.
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Found device /dev/mmcblk1p1.
Starting File System Check on /dev/mmcblk1p1...
[ OK ] Finished Enable and configure wl18xx bluetooth stack.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston, a Wayland compositor, as a system service...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ OK ] Finished File System Check on /dev/mmcblk1p1.
Mounting /run/media/boot-mmcblk1p1...
[ OK ] Mounted /run/media/boot-mmcblk1p1.
[FAILED] Failed to start Weston, a Wayland compositor, as a system service.
See 'systemctl status weston.service' for details.
[2024-11-21 11:19:55
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
[ OK ] Started containerd container runtime.
[2024-11-21 11:19:56
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
adwaita-icon-theme-symbolic
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gnu-config
grub-common
grub-editenv
grub-efi
gzip
hidapi
kbd-dev
kbd-keymaps-pine
less
libasm1
libatomic-dev
libatomic1
libbfd
libdebuginfod1
libdw1
libelf1
libgcc-s-dev
libgcc1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libopcodes
libqt5charts-examples
libqt5charts-plugins
libqt5charts-qmlplugins
libqt5charts5
libqt5serialport-examples
libqt5serialport-plugins
libqt5serialport-qmlplugins
libqt5serialport5
libqt5svg-examples
libqt5svg-plugins
libqt5svg-qmlplugins
libqt5svg5
libqt5virtualkeyboard-plugins
libqt5virtualkeyboard-qmlplugins
libqt5virtualkeyboard5
libreadline-dev
libreadline8
libstdc++-dev
libstdc++6
libunistring5
m4
make
nettle
parted
piglit
qt3d-plugins
qt3d-qmlplugins
qt3d
qtbase-examples
qtbase-plugins
qtbase-qmlplugins
qtbase
qtconnectivity-plugins
qtconnectivity-qmlplugins
qtconnectivity
qtdeclarative-plugins
qtdeclarative-qmlplugins
qtdeclarative-tools
qtdeclarative
qtgraphicaleffects-qmlplugins
qtlocation-examples
qtlocation-plugins
qtlocation-qmlplugins
qtlocation
qtmultimedia-examples
qtmultimedia-plugins
qtmultimedia-qmlplugins
qtmultimedia
qtquics-qmlplugins.control
qtquics2-plugins.control
qtquics2-qmlplugins.control
qtquics2.control
qtscript-examples
qtscript-plugins
qtscript-qmlplugins
qtscript
qtwayland-examples
qtwayland-plugins
qtwayland-qmlplugins
qtwayland
tar
which
If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Finished Print notice about GPLv3 packages.
[ OK ] Reached target Multi-User System.
[ OK ] Reached target Graphical Interface.
Starting Record Runlevel Change in UTMP...
[ OK ] Finished Record Runlevel Change in UTMP.
[2024-11-21 11:19:58
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project j7200-evm ttyS2
Arago 2023.10 j7200-evm ttyS2
j7200-evm login: [ 20.444623] platform can-phy3: deferred probe pending
[2024-11-21 11:20:03
[ 20.449681] platform 2731000.can: deferred probe pending
[ 20.454988] platform 2910000.pcie: deferred probe pending
[ 20.460386] platform mux-controller-0: deferred probe pending
[ 20.466125] platform mux-controller-1: deferred probe pending
[2024-11-21 12:20:19
Can you help us to find out what is wrong?
Best Regards!