Tool/software:
HI!
Does each AM623 EQEP modules only provide one compare register?

There is no way to apply, perhaps a shadow register, that does something similar:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
HI!
Does each AM623 EQEP modules only provide one compare register?

There is no way to apply, perhaps a shadow register, that does something similar:

Hello
Rafael Volkmer
Thank you for the query.
I need to check with the team internally.
Please expect delay in response given the holiday week.
Regards,
Sreenivasa
Hello Rafael Volkmer
Pls refer below input i received as a possible suggestion:
[The following is a suggestion rather than a tested solution]
However, It may be possible using two cascaded ECAP peripherals (must be sequential instances) The sync could be configured so that both counters are reset/loaded at the same time. Signal A could go to the first ECAP and signal B to the second. The delta between the signals could then be calculated base on the capture timer values multiplied by the timer period.
Something like this:

EPWM can be configures in a similar manner
Regards,
Sreenivasa