Part Number: AM5706
Tool/software:
Hi
Thanks for the previous support.
Previous Link : e2e.ti.com/.../am5706-pcie-endpoint-runtime-failure
We resolved the PCIE run time link failure issue successfully for the system where only one controller is being used.
But Now we are facing the same issue with another LRU in which we are using both the PCIE controllers available. We are using both the controller as endpoint and both of them are connected to 2 different Intel processor. We have already disabled the NSR bit as discussed in previous thread. But now if the link failure is happening the default value is as below
0x51800044 --> 0x8 (Default initial configuration)
0x51800044 --> 0x0 (After Link Down)
Same state transition is observed here as before. We are trying to find out how the NSR bit is getting enabled where during initialization I m disabling this bit.
Can you please give some information for below registers
PCIECTRL_EP_DBICS2_PM_CSR RW 0x5100 1044
PCIECTRL_EP_DBICS_PM_CSR RW 0x5100 0044
So please help us resolve this issue.
Note : All the information regarding this is available in previous thread. If any further information is required please let me know.