This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Technical Support - Beagleboards XM Rev C - Need Consultant that can bring boards up with Android



I have 2 Beagleboards XM Rev C that I can not make them work with TI_Android_GingerBread_2_3_4_DevKit_2_1.tar.gz.  Is there a place or person in Los Angeles California that I can take the boards to?   

  • Hi Carlos,

    1. I think you are facing this issue since long back. I thought it was solved by the thread we were discussing last time.

    2. Anyways,

    Location you have mentioned, it might bit difficult but I will try to get some contact nearby if I can.

    3. R u facing still red screen issue ? Or some boot issue ? Could you send us complete boot log + logcat + screen capture + cmd arguments again

    4. If you are able to boot the board, then try to connect ADB and capture the screen shot.

    BR,

    satish

  • Hi Satish,

    I am not working on this problem full time. I have one board that the serial port stop working. it just spews 60606060. Have no clue why. The other board behaves differently depending if I use Froyo o Gingerbread. It just does not finish booting.  If you can get me someone local (Los Angeles CA area)  that I can go to I will pay for the services. I will attempt to boot again this weekend.  I am using a virtual machine running Ubuntu. That may be the problem. Thanks