This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

looking for recommended trace impedance and termination values for C6678 DDR3 interface

The evaluation board for the C6678 use 51 Ohm for termination resistors. It is hard to decide what to use without having to spend a lot of time and simulation. I would like to know what TI would recommend for termination values. I am sure some value between 51 and 39.9 ohm will work but it may degrade the interface just a little bit more if improperly selected. I also need to know what the recommended trace impedances should be for maximum performance.

 

Best Regards,
John