Part Number: SK-AM69
Tool/software:
Hello,
I have been trying to get our graphical application (using SDL and GLES) to run on the SK-AM69 evaluation board using Yocto (scarthgap) and the meta-ti-bsp layer. I am using Weston and I have been able to boot into that, but I have been running into issues trying to create a window with SDL, getting the following error:
wl_drm@19: error 0: authenticate failed
To test whether this was an issue with our program, I tried to just get the kmscube program running, and got the following DRM error:
no connected connector! failed to initialize legacy DRM
My build/conf/local.conf just trying to run kmscube looks like:
IMAGE_INSTALL:append = " ti-img-rogue-umlibs ti-img-rogue-driver"
PREFERRED_PROVIDER_virtual/gpudriver = "ti-img-rogue-driver"
DISTRO_FEATURES:append = " systemd pam"
INIT_MANAGER = "systemd"
DISTRO_FEATURES:remove = " vulkan"
DISTRO_FEATURES:append = " opengl"
IMAGE_INSTALL:append = " libdrm"
IMAGE_INSTALL:append = " kmscube"
PACKAGECONFIG:append:pn-libsdl2 = " gles2 kmsdrm arm-neon"
PACKAGECONFIG:append:pn-weston = " kms egl wayland"
PACKAGECONFIG:append:pn-mesa = " gbm egl"
MACHINE_ESSENTIAL_EXTRA_RRECOMMENDS += "kernel-modules"
MACHINE ??= "am69-sk"
I just wanted to check whether I had done anything wrong in my configuration with regards to the board, or missed any necessary installs onto the image, or whether this is an issue with drivers?
Thanks