This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMX to restart/reset encode buffer



Hello,

What I am trying to do would seem straightforward, but I am having a lot of trouble. I have the encoder running and it outputs the buffer to a file.  This works fine for me. However, I would like for it to start a new file after 10 frames.This does not work for me.

 

Simplified, this is what I have:

while (1)
{
    //Read filled buffer pointer from the pipe
    framecounter++;
    read (encILComp->outPortParams->opBufPipe[0], &pBufferOut, sizeof (pBufferOut));
   
     //Every 10 frames
    if(frameCounter % 10)
    {

        // Close this file and start a new one.

       sprintf (filename, "/dev/shm/%d.264", frameCounter/10);
       fclose(fp);
       FILE * fp = fopen(filename, "w+");
    }
      

        // Write frame to file
    fwrite (pBufferOut->pBuffer, sizeof (char), pBufferOut->nFilledLen, fpFile);
      
        // Pass the input buffer to the component for next frame
    err = OMX_FillThisBuffer (encILComp->handle, pBufferOut);

}

This only works on the first file generated. All the other files VLC cannot play. I suspect the encoder puts information in to the first buffer that VLC needs to play, and the remaining frames do not have it. In my closing/opening section, I need to tell OMX to start over or find some other fix.

 

Is there an OMX call to tell the encoder to start a new file or resend the information that VLC needs?

 

Thanks,
Dan