Hello,
I'm trying to run the norflash test that came with the spectrum EVM test package. To run the test, I prevent the system from booting by putting it in bootmode 0. Using CCSv5, I load evm816x.gel file and then the norflash.out file. The test will always hang at erasing sectors.
I tried the DDR test and the EEPROM test and both work fine. I do have the IO Expansion Daughter board connected.
Have anyone at TI verified that this NOR flash test is working? What do I have to do to get it to work? Below is the test output. Thanks.
[CortexA8] 01 Testing NOR Flash...
[CortexA8] 1
[CortexA8] This test writes writes to the entire first sector then writes a 1024-byte long pattern for each address line.
[CortexA8] Manufacture ID : 0x0090
[CortexA8] Device ID1 : 0x0090
[CortexA8] Device ID2 : 0x0090
[CortexA8] Device ID3 : 0x0090
[CortexA8] Erasing Sectors to be written to.