Part Number: AM623
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
The test of the FlashROM connected to the custom board does not pass.
Custom board with AM62 mounted is now booted in SD boot mode.
The sample project of OSPI_FLASH_IO was modified.
Test passed for 1S-1S-1S, but cannot pass for 4S-4S-4S protocol.
I think there is a problem with the settings on Sysconfig, but I don't know what the problem is.
【Device Information】
・CPU:AM6234ATCGHAALW
・FlashROM:MT25QL256ABA8ESF
-256Mbit
-Quad SPI
I had already inquired about this, but I would like to make a new inquiry.
The settings for Flash in sysconfig's "ti_board_oepn_close.c" are as follows.
/*
* FLASH
*/
/* FLASH Object - initialized during Flash_open() */
Flash_NorOspiObject gFlashObject_MT25QL256ABA8ESF =
{
.rdDummyValPhyMode = FLASH_NOR_UPDATE_RD_DUMMY_VALUE,
};
/* FLASH Attrs */
Flash_Attrs gFlashAttrs_MT25QL256ABA8ESF =
{
.flashType = CONFIG_FLASH_TYPE_SERIAL,
.flashName = "MT25QL256ABA8ESF",
.deviceId = 0xBA19,
.manufacturerId = 0x20,
.flashSize = 33554432,
.blockCount = 1024,
.blockSize = 32768,
.pageCount = 128,
.pageSize = 256,
.sectorCount = 8192,
.sectorSize = 4096,
};
/* FLASH DevConfig */
Flash_DevConfig gFlashDevCfg_MT25QL256ABA8ESF =
{
.cmdExtType = OSPI_CMD_EXT_TYPE_REPEAT,
.enable4BAddr = FALSE,
.addrByteSupport = 1,
.fourByteAddrEnSeq = 0xA0,
.cmdWren = 0x06,
.cmdRdsr = 0x05,
.cmdWrsr = 0x00,
.srWip = (1 << 0),
.srWel = (1 << 1),
.xspiWipRdCmd = 0x85,
.xspiWipReg = 0x00800000,
.xspiWipBit = (1 << 0),
.resetType = 0x10,
.eraseCfg = {
.blockSize = 32768,
.sectorSize = 4096,
.cmdBlockErase3B = 0x52,
.cmdBlockErase4B = 0x52,
.cmdSectorErase3B = 0x20,
.cmdSectorErase4B = 0x20,
.cmdChipErase = 0xC7,
},
.idCfg = {
.cmd = 0x9F, /* Constant */
.numBytes = 3,
.dummy4 = 0,
.dummy8 = 0,
},
.protocolCfg = {
.protocol = FLASH_CFG_PROTO_4S_4S_4S,
.isDtr = FALSE,
.cmdRd = 0x6B,
.cmdWr = 0x02,
.modeClksCmd = 0,
.modeClksRd = 0,
.dummyClksCmd = 10,
.dummyClksRd = 10,
.enableType = 0,
.enableSeq = 0x00,
.protoCfg = {
.isAddrReg = FALSE,
.cmdRegRd = 0x6B,
.cmdRegWr = 0x02,
.cfgReg = 0x00,
.shift = 0,
.mask = 0x00,
.cfgRegBitP = 0,
},
.strDtrCfg = {
.isAddrReg = TRUE,
.cmdRegRd = 0x85,
.cmdRegWr = 0xB1,
.cfgReg = 0x00800006,
.shift = 1,
.mask = 0x02,
.cfgRegBitP = 1,
},
.dummyCfg = {
.isAddrReg = FALSE,
.cmdRegRd = 0x85,
.cmdRegWr = 0xB1,
.cfgReg = 0x00,
.shift = 0,
.mask = 0x00,
.cfgRegBitP = 0,
},
},
.flashWriteTimeout = 512,
.flashBusyTimeout = 256000000,
};