Part Number: DRA821U
Other Parts Discussed in Thread: DRA821
Tool/software:
Hello, I have to ask for your help.
about DRA821U, there is MAIN Domain and MCU Domain, if one Ethernet Port is connected with MAIN Domain, another Ethernet Port is connected with MCU Domain, can the two Ethernet Port work at the same time? in my ideal, if two Ethernet Ports are connected with MAIN Domain, the two ethernet ports can not run at the same time, because there is a switch, am i right? but if one Ethernet Port is connected with MAIN Domain, another Ethernet Port is connected with MCU Domain, the two ethernet ports can run at the same time, because the two ethernet ports controlled by different MCU, there are two switchs, am i right?